FAQ: What is the size of the hole marked A in the N6700/N8700 dimension drawing?

These holes are 10-32 PEMS. Screw length travel into the side of the product should be limited to 0.250”. This will guarantee complete engagement of the PEM, leaving approx. three complete threads exiting the internal side of the PEM. Screws longer than 0.250” can damage the unit.

Applies to: N5740A, N5741A, N5742A, N5743A, N5744A, N5745A, N5746A, N5747A, N5748A, N5749A, N5750A, N5751A, N5752A, N5761A, N5762A, N5763A, N5764A, N5765A, N5766A, N5767A, N5768A, N5769A, N5770A, N5771A, N5772A

Applies to: N8731A, N8732A, N8733A, N8734A, N8735A, N8736A, N8737A, N8738A, N8739A, N8740A, N8741A, N8742A, N8754A, N8755A, N8756A, N8757A, N8758A, N8759A, N8760A, N8761A, N8762A

Select Home to return to the table of contents for more FAQs.

Visit our Power Products Forum for additional topics and discussions.

Read technical postings on our Power Blog – Watt’s Up?